With increasing regulations prompting a shift toward sustainable alternative refrigerants, retailers are looking more closely at CO2 transcritical booster systems to anchor their refrigeration operations, even in warmer climates. Sprouts Farmers Market is among the first retailers in North America to do just that. They opened their first store in suburban Atlanta in July 2014, and when they did, they set out to prove CO2 transcritical booster systems aren’t only for cool climates.
Like many food retailers, Sprouts has historically employed more traditional refrigeration systems based on common hydrofluorocarbon (HFC) refrigerants. These HFC systems operate with what’s traditionally seen as acceptable temperatures and pressures. CO2’s low critical point temperature and high operating pressure (around 1,500 psig) are characteristically not found in traditional HFC-based refrigeration. These are the primary reasons for the reluctance to move toward CO2. But, with advances in system technology and architecture, CO2 can be a game changer for retailers seeking to improve energy efficiencies, achieve sustainability targets and cross the finish line on regulatory compliance.
Changing their refrigeration philosophy and moving to a CO2 transcritical system architecture was a giant step for Sprouts, especially for this store in the hot, humid climate of Atlanta. To pull this off, they turned to OEM partner Hillphoenix, and Hillphoenix, seeing the challenge presented by installing a CO2 transcritical booster system in a warm climate, turned to Emerson.
Emerson’s E2 facility management system was installed to oversee the CO2 transcritical booster system. It manages nearly 50 electronic case control units and optimizes the facility’s overall energy management profile.
The E2 system helps improve performance in multiple ways:
-
- Controls the variable speed of the fans on the adiabatic condenser in response to operating conditions
- Optimizes compressor coefficient of performance by regulating system discharge pressures via Emerson’s high-pressure CO2controller
- Provides complete oil management control of all CO2refrigeration compressors
- Communicates with and captures information from individual case control units
- Provides complete control of building HVAC and refrigeration systems, and supports the retailer’s energy and maintenance reduction strategies

Warm climate CO2-based transcritical booster system installation
The E2 system also allows Sprouts operators to run diagnostics, monitor the system remotely through Emerson’s Service Center and, if necessary, shut down the system components before failure.
The condenser manages both low- and medium-temperature refrigeration requirements on the same system using only CO2 as the refrigerant, another unique aspect to the transcritical booster system. Running both requirements from the same condenser enhances the efficiency of the system across the store.
It’s understandable why stateside end users are hesitant to switch to CO2 transcritical booster systems. Concerns over operating pressures, maintenance levels and energy have prompted careful and steady evaluations to understand the true cost of ownership for their enterprises. Emerson technology helped ease those concerns for Sprouts. Their Atlanta-area store is operating efficiently and effectively on the transcritical system.
This blog is a summary of the article National Grocery Store Chain Makes Transition to Transcritical Refrigeration from our recent edition of E360 Outlook.

Join Emerson and NASRC for Free CO2 Training
Service technicians are at the front lines of the refrigerant transition in HVACR. As part of our...

The HSI Furnace Control that Keeps HVACR Pros at the Jobsite, Not the Supply House — An HVAC School Podcast Recap
In the dead of winter, there are few things more frustrating to a homeowner than waking up to a...

Understanding A2L Refrigerant Fundamentals — New Blog and Video Series
A2L refrigerants are a new and relatively unknown commodity in the U.S. commercial refrigeration...