As essential businesses, food retailers were among the few sectors that had remained open during the early stages of the coronavirus pandemic. Staying open meant they would have to adapt quickly to new operating protocols, which often included one-way aisles, plexiglass shields at registers and enhanced cleaning procedures. Grocers were also inundated with high volumes of click-and-collect orders, which tested their e-fulfillment capabilities and presented additional challenges. I recently contributed to an ACHR News article discussing the shifting grocery landscape and its potential impacts on store and refrigeration system designs.

Attempts to provide “contactless” shopping experiences were among the first areas of focus, as store layouts were modified to limit the need to touch physical items and surfaces. While these were originally intended as stop-gap strategies, some of these short-term measures have already become more permanent elements of in-store designs. In fact, new store builds and remodels will likely feature layouts and case placements that are designed to adhere to as many safeguards as possible and provide much-needed merchandizing flexibility.
Of course, this shift will also affect the type of refrigeration architectures grocers select to address these emerging challenges. Flexibility in refrigeration translates first into the ability to meet typical capacities, but also provides the freedom to scale up or down to meet fluctuations in demand — such as staging additional self-contained cases or enabling variable-capacity modulation in walk-in units that support click-and-collect.
Shoring up stores for click-and-collect
While demand for click-and-collect fulfillment surged significantly during the initial onset of the pandemic, months later it shows little to no signs of letting up. In fact, recent reports indicate a 23 percent growth in click-and-collect adoption from June to July. Many experts believe this change in consumer behavior will represent a more permanent change in buying habits — although the degree to which it becomes a preferred shopping method remains to be seen.
Fortunately for most major retailers, click-and-collect capabilities have been in place for several years. But that doesn’t mean they were necessarily prepared for pandemic-level order volumes. In terms of fulfillment and execution, this emerging business model presents a variety of cold storage, picking and associated labor requirements.
As retailers respond to the increased amount of online shopping, they will need to account for fluctuations in consumer demand and the impacts on refrigeration equipment loads. Refrigeration design strategies with variable-capacity modulating compressors — such as the Copeland™ digital outdoor refrigeration unit, X-Line Series and Copeland scroll compressors — will help retailers balance click-and-collect refrigeration loads more effectively.
Another effective strategy is to implement “dark stores,” which are dedicated online fulfillment centers. Retailers who operate dark stores essentially take load fluctuations from click-and-collect activities out of the equation, which may make it easier to balance refrigeration loads. Whichever method is preferred, retailers will ultimately approach click-and-collect services differently, depending on their local demographics and store design strategies.

Evaluating the ROI of Supermarket Sustainability Efforts
The spectrum of supermarket sustainability concerns has expanded significantly in recent years. As...

Seven Keys to Demystifying CO2 Refrigeration
The U.S. commercial refrigeration market is poised for a surge in the use of CO2 (R-744) as a...

Tools for Delivering Perishable Food Freshness This Holiday Season
More than any time of year, food is a central attraction of the holiday season. Sharing, preparing...