ACHR News recently interviewed me for an article titled “Compressor Retrofits on the Rise in Commercial Refrigeration.” It featured a variety of perspectives on the merits of compressor retrofits versus total system replacement. The article can be found here.

When facility energy costs creep up, one of the first suspects is almost always the commercial refrigeration system. It’s a reasonable assumption to make. Over time, it’s very common for energy efficiency to decline as systems drift from their original commissioned performance baselines.
But that doesn’t make a total system replacement inevitable. Many food retailers are reclaiming energy efficiencies by pairing system recommissioning with a measurement and verification (M&V) program and targeted compressor upgrades. In the process, they can reduce energy consumption, improve system performance and reliability and extend the system’s lifespan without the capital investment and business interruption that a full system replacement would require.
Back to the (factory spec) basics
Prolonged use, normal wear and tear and migration from recommended setpoints can degrade efficiency over time. Recommissioning fine-tunes the refrigeration system so that it operates as intended. The process typically involves optimizing every setpoint, cleaning condensers and replacing damaged components. Often, operators can capture significant savings just by recalibrating their system to factory specifications.
Implementing an M&V program ensures those savings are sustainable. Energy-monitoring equipment that delivers real-time insights will help operators ensure their equipment stays in tune. When variances occur, contractors can quickly identify the root cause and address the issue. But just as important, they can use the data generated by the M&V program to make informed decisions on future improvements.
Greater efficiency through variable-capacity modulation
The next step is to enhance energy efficiencies in low- and medium-temperature racks by upgrading to a digital compressor with variable-capacity modulation or by adding a variable frequency drive (VFD). Often, the best candidates for replacement are fixed-capacity compressors that are underperforming or the smallest displacement compressors in each rack.
By adding a variable-capacity digital compressor or VFD to the mix, operators can:
-
- Accurately match capacity to changing refrigeration loads
- Improve case temperature precision
- Reduce compressor cycling
- Maintain tighter control over suction manifold pressures
One often overlooked solution is the option to add a VFD to legacy Copeland™ Discus™ and Copeland™ fixed-capacity scroll compressors. Perhaps a more common solution is replacing one or even two underperforming fixed-capacity compressors with a digital compressor such as a Copeland Discus digital or Copeland digital scroll compressor — both of which enable variable-capacity modulation to deliver significant energy savings.
When a leading supermarket chain tested the strategy on a 20-year-old, 45,000 square foot grocery store in Ontario, it found that:
-
- Recommissioning reduced energy costs by 18%
- Replacing two weaker units with Copeland Discus compressors reduced energy costs by an additional 16% and qualified the retailer for a local energy incentive program
The entire effort delivered an annual energy savings of more than $40,000.
Proven strategies for every situation
As other contributors to the article note, compressor upgrades (or retrofits) may not always be the right solution for every system. Depending on the age and condition of the equipment, a total system replacement may make more financial sense. This strategy would ensure all system controls and components are integrated and optimized for lower-GWP refrigerants.
Ultimately, choosing between a compressor retrofit or full system replacement should be a data-driven decision that operators make in consultation with their contractors. As a leader in commercial refrigeration and other cold chain technologies, Emerson can help operators maximize their return on that decision. We offer a full suite of components that boost energy efficiency and provide internet of things (IoT) capabilities for retrofits and new equipment alike. Our application engineers are available to answer questions related to refrigeration system performance, retrofit opportunities and strategies for maximizing energy efficiency.

Understanding A2L Refrigerant Fundamentals — New Blog and Video Series
A2L refrigerants are a new and relatively unknown commodity in the U.S. commercial refrigeration...

New EPA Proposal Drives Regulation of HFC Phasedown in HVACR
Since the passing of the American Innovation & Manufacturing Act (AIM Act) in 2020, the HVACR...
![[Webinar Recap] The Growing Case for CO2 Refrigeration](https://e360blog.emerson.com/wp-content/uploads/2022/09/14470_E360_CO2Landscape_OnDemand_960x600-1.jpg)
[Webinar Recap] The Growing Case for CO2 Refrigeration
When we consider the emerging class of low-global warming potential (GWP) refrigerants, the...